The following documentations describe the communication of TwinCAT with external devices.
Example |
Description |
Crestron |
Communication with Crestron Controls. |
sACN 2016 |
Transmitting DMX data as a complete universe embedded in an sACN frame. (sACN standard, E1.31-2016 and use of TwinCAT 3) |
sACN 2009 |
Transmitting DMX data as a complete universe embedded in an sACN frame. (sACN standard, E1.31-2009 and use of TwinCAT 2) |
ArtNet |
Transmitting DMX data as a complete universe embedded in an ArtNet frame. |
Kinect |
Communication to Microsofts Kinect Sensor |
PosiStageNet |
protocol specification for transmitting position data |
PJLink |
Communication protocol based on TCP/IP. |
QRC |
Communication protocol in Q-SYS. |