Beckhoff TwinCAT Supplement
BECKHOFF Information System 1:

TwinCAT Supplement - Product overview

Category System
Productnumber Productname Description
TS1110 TwinCAT Simulation Manager Powerful tool for simulating machines or machine systems.
TS1120 TwinCAT ECAD Import Softwaretool for importing XML files from the ECAD systems. A TwinCAT System Manager configuration and a PLC program are created automatically.
TS1140 TwinCAT Management Server Software package for administration of Beckhoff controls.
TS1150 TwinCAT Backup Server for backing up and restoring complete PCs that already have an operating system installed.
TS1600 TwinCAT Engineering Interface (ENI) Server Software package for version control management and multi-user PLC development
TS1800 TwinCAT PLC HMI TwinCAT PLC Visualization
TS1800-0030 TwinCAT PLC HMI CE TwinCAT PLC Visualization under CE
TS1810 TwinCAT PLC HMI_Web TwinCAT PLC Web Visualization

 

Category Measurement
Productnumber Productname Description
TS3300 TwinCAT Scope2 Software Scope
TS3900 TwinCAT Solar Position Algorithm Library with function blocks for  determination of the position of the sun.

 

Category Motion
Productnumber Productname Description
TS1500 TwinCAT Valve Diagram Editor Softwaretool to develop the characteristic curve for a hydraulic valve (Installation routine).
TS1510 TwinCAT Cam Design Tool Softwaretool to develop electronic cam plates on the basis of VDI guideline 2143 (Installation routine) 
TS5050 TwinCAT NC Camming Softwaretool to synchronise two or more axes.
A master axis is then actively controlled, and the position of one or more coupled slave axes is synchronously controlled by the nc.
TS5055 TwinCAT NC Flying Saw Softwaretool to synchronise the position and the speed of tool and workpiece.
TS5060 TwinCAT NC FIFO Axes Softwaretool to synchronise two or more axes.
In this case, rather than having one master-slave table prescribed in advanc, the latest axis positions are constantly "topped up" by a PLC program.
TS5065 TwinCAT PLC Motion Control  XFC Library with function blocks relevant to realise digital cam switches.
TS5066 TwinCAT PLC Remote Syncronisation Library to synchronize distributed systems.
TS5070 TwinCAT PackAL Library with functionblocks relevant for packaging applications
TS5110 - TS5112 TwinCAT Kinematic Transformation Software package that integrates itself transparently into the existing Motion Control world of TwinCAT
TS5800 TwinCAT Digital Cam Server Fast camshaft controller as software implementation in TwinCAT, freely configurable via the TwinCAT System Manager.
TS5810 TwinCAT PLC Hydraulics V3 Library with functionblocks relevant for hydraulic axes.


Category Communication
Productnumber Productname Description
TS6000 TwinCAT ADS Communication Library TwinCAT ADS Communication Library contains ADS components  to implement ADS applications.
TS6100 TwinCAT OPC UA_Server Standard interface for the communication in the Automation technology
TS6100-0030 TwinCAT OPC UA Server CE TwinCAT OPC Server (DataAccess 1.0a & 2.0 / Alarm&Events 1.0 / XML-DA )
Standard interface for the communication in the Automation technology   for CE platform.
TS6120 TwinCAT OPC Server TwinCAT OPC Server (DataAccess 1.0a & 2.0 / Alarm&Events 1.0 / XML-DA )
Standard interface for the communication in the Automation technology  
TS6120-0030 TwinCAT OPC Server CE TwinCAT OPC Server (DataAccess 1.0a & 2.0 / Alarm&Events 1.0 / XML-DA )
Standard interface for the communication in the Automation technology  for CE-platform.
TS6220 - TS6222 TwinCAT  EtherCAT Redundancy Software module to expand the EtherCAT-Master to a redundancy from 250 to more than 1000 slaves
TS6250 TwinCAT Modbus TCP Server Software package for communication with Modbus Client resp. Modbus Server via Modbus TCP.
TS6250-0030 TwinCAT Modbus TCP Server CE Software package for communication with Modbus Client resp. Modbus Server via Modbus TCP for CE platform.
TS6255 TwinCAT PLC Modbus RTU Library with function blocks for serial communication with Modbus end devices.
TS6270-0030 TwinCAT PROFINET  Device (Slave) Software for integrating TwinCAT controllers as slave device into a Profinet network
TS6271-0030 TwinCAT PROFINET Controller Software for integrating TwinCAT controllers as master device into a Profinet network
TS6280 TwinCAT Ethernet/IP Slave Software for integrating TwinCAT controllers as slave device into an EtherNet/IP network
TS6280-0030 TwinCAT Ethernet/IP Slave CE Software for integrating TwinCAT controllers based on Windows CE as slave device into an EtherNet/IP network
TS6300 TwinCAT FTP Client Software package that enables the TwinCAT PLC to access several FTP server.
TS6310 TwinCAT TCP/IP Server Software package for implementation one or several TCP/IP-Server/-Clients.
TS6310-0030 TwinCAT TCP/IP Server CE Software package for implementation one or several TCP/IP-Server/-Clients for CE platform.
TS6340 TwinCAT PLC Serial Communication Library with function blocks for serial communication via bus terminals or PC serial port.
TS6341 TwinCAT PLC Serial Communication 3694R-RK512 Library with function blocks for serial communication with 3964R and RK512 protocol via bus terminals or PC serial port.
TS6350 TwinCAT SMS/SMTP Server Software package and library with function blocks for sending SMS messages via bus terminals or PC serial port.
TS6350-0030 TwinCAT SMS/SMTP Server CE Software package and library with function blocks for sending SMS messages via bus terminals or PC serial port, for CE platform.
TS6360 TwinCAT Virtual Serial COM Driver Driver to access RS232/RS485 EtherCAT bus terminals (EL6001, EL6021) as virtual serial ports (COM ports)
TS6370 TwinCAT DriveCom OPC Server Standard interface to configure Siemens 611U and Siemens Posmo drives
TS6371 TwinCAT DriveTop Server The server enables easy communication to DriveTop compatible drives.
TS6420 TwinCAT DataBase Server Software package for communication with a database.
TS6420-0030 TwinCAT DataBase Server CE Software package for communication with a database for the CE platform.
TS6421 TwinCAT XML Data Server Software for initialisation of TwinCAT PLC Variables with data, which are stored in a XML file. 
TS6421-0030 TwinCAT XML Data Server CE Software for initialisation of TwinCAT PLC Variables with data, which are stored in a XML file, for CE platform. 
  TwinCAT PLC Modular Device Profile Library with function blocks for access to MDP (Modular Device Profile) information (part of IPC-diagnosis).
TS6500 TwinCAT PLC-IEC-60870-5-101 Master Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-101.
TS6501 TwinCAT PLC-IEC-60870-5-101 Slave Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-101.
TS6502 TwinCAT PLC-IEC-60870-5-102 Master Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-102.
TS6504 TwinCAT PLC-IEC-60870-5-103 Master Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-103.
TS6506 TwinCAT PLC-IEC-60870-5-104 Master Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-104.
TS6506-0030 TwinCAT PLC-IEC-60870-5-104 Master CE Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-104 for CE platform.
TS6507 TwinCAT PLC-IEC-60870-5-104 Slave Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-104.
TS6507-0030 TwinCAT PLC-IEC-60870-5-104 Slave CE Library with function blocks for communication via the telecontrol protocol according to IEC60870-5-104 for CE platform.
TS6600 TwinCAT PLC RFID Reader Communication Library for communication with RFID readern from PLC.
TS6610 TwinCAT PLC S5/S7 Communication Library with function blocks for serial communication between local TwinCAT PLC and S5/S7 controller via Ethernet.

 

Category Control
Productnumber Productname Description
TS4100 TwinCAT PLC Controller Toolbox Library with function blocks for solving control tasks.
TS4110 TwinCAT PLC Temperature Controller Library with functionblocks for monitoring and controlling temperature-dependent processes.

 

Category Building Automation
Productnumber Productname Description
Ts8000 TwinCAT PLC HVAC Library with functionblocks for automation of buildings for heating, ventilation, air conditioning and sanitary systems.
TS8010 TwinCAT PLC Building Automation Basic Library with function blocks for Building Automation.
TS8020 TwinCAT BACnet/IP Communication protocol for Building Automation.Part of TwinCAT installation.
TS8035 TwinCAT FIAS Server Software package with access to systems according to the FIAS standard.
TS8036 TwinCAT Crestron Server Software package for communication with Crestron Controller
TS8037 TwinCAT Bang & Olufsen Server Software package for accessing the B&O Masterlink Gateway.
TS8040 TwinCAT BA Software suite for Building Automation
TS8100 TwinCAT Building Automation Framework Software package as framework for own Building Automation PLC projects
  TwinCAT PLC DALI Library for communication with the DALI Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC DMX Library for communication with the DMX Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC EnOcean Library for communication with the EnOcean Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC EIB Library for communication with the EIB Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC LON Library for communication with the LON Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC M-Bus Library for communication with the M-Bus Bus Terminal (is delivered with TwinCAT)
  TwinCAT PLC MP-Bus Library for communication with the MP-Bus Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC SMI Library for communication with the SMI Bus Terminal (is delivered with TwinCAT).
  TwinCAT PLC GENIbus Library for communication via the GENIbus protocol (is delivered with TwinCAT).